cancel
Showing results for 
Search instead for 
Did you mean: 

我使用最新版的STM32CodeMX和TM32CubeF4 Firmware Package V1.24.1生�?IAR V7工程编译时出现两个错误,

�?�
Associate
 
3 REPLIES 3
Imen.D
ST Employee

Hello,

Please, posting your question in English, so that it will be clearer.

Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

"I used the latest version of STM32CodeMX and STM32CubeF4 Firmware Package V1.24.1 to generate two errors when compiling IAR V7 projects."

I guess the question would relate to if it needs IAR V8, or what specific errors are actually being reporting, and addressing the cause(s) of those errors.

What version of IAR is ST testing with?

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
Hello,
When I generate the IAR V7 code by STM32CubeMX5.2.1 and TM32CubeF4 Firmware Package V1.24.1,Two errors occurred.
The first,Fatal Error[Pe035]: #error directive: intrinsics.h is already included previously! E:\AC_Project\AC_Project0506\Drivers\CMSIS\Include\cmsis_iccarm.h 483 。
The second,the IAR V7 can not recognizable “__restrict�?
#ifndef __RESTRICT
#define __RESTRICT __restrict
#endif

Looking forward to your help,Thank you.