cancel
Showing results for 
Search instead for 
Did you mean: 

Hello Sir Is CR95HF support sony FeliCa function? if yes, any software library or samples available for reference? if Not, which part can support Felica? Thank you.

VHo
Associate

Hello Sir

Is CR95HF support sony FeliCa function? if yes, any software library or samples available for reference? if Not, which part can support Felica?

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions
Brian TIDAL
ST Employee

​Hi,

the following readers of the ST25R family provide NFC-F / FeliCa™ reader mode support:

  • ST25R95/CR95HF/ST95HF NFC/HF RFID Reader IC
  • ST25R3911B NFC / HF RFID Reader IC
  • ST25R3916 High performance NFC universal device and EMVCo reader

Note: for new developments, ST recommends to use ST25R95 in replacement of CR95HF/ST95HF (see your local ST representative for further information).

ST25R95 is the convergence device for CR95HF and ST95HF. 

A demo of ST25R95/CR95HF/ST95HF reader features (polling tags for various technologies including NFC-F and displaying UID) is included in the X-CUBE-NFC3 v2.0.0 package. This package provides an RF Abstraction Layer common with other readers of the ST25R family.

This software package is ready to run on X-NUCLEO-NFC03A1 expansion board with either NUCLEO-L476RG, NUCLEO-F401RE or NUCLEO-F103RB STM32 boards.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Brian TIDAL
ST Employee

​Hi,

the following readers of the ST25R family provide NFC-F / FeliCa™ reader mode support:

  • ST25R95/CR95HF/ST95HF NFC/HF RFID Reader IC
  • ST25R3911B NFC / HF RFID Reader IC
  • ST25R3916 High performance NFC universal device and EMVCo reader

Note: for new developments, ST recommends to use ST25R95 in replacement of CR95HF/ST95HF (see your local ST representative for further information).

ST25R95 is the convergence device for CR95HF and ST95HF. 

A demo of ST25R95/CR95HF/ST95HF reader features (polling tags for various technologies including NFC-F and displaying UID) is included in the X-CUBE-NFC3 v2.0.0 package. This package provides an RF Abstraction Layer common with other readers of the ST25R family.

This software package is ready to run on X-NUCLEO-NFC03A1 expansion board with either NUCLEO-L476RG, NUCLEO-F401RE or NUCLEO-F103RB STM32 boards.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.