2019-05-22 01:08 AM
Hi ,
I'm trying to read the accelerometer data from the LIS2DH12TR which is connected to CC1310 TI's Controller.
In my design I'm using I2C hence i have connected the CS pin to Vdd(3.3V) and SA0 pin to VDD. As per the Data sheet with my case the address will be 0x19(SA0 is connected to Vdd).
I'm able to initialize the I2C and while reading the Data it always prints all values to zero except the Out_Z(H & L) and Out_H and Out_L are 255(Out_Z= accelerometer values in the z direction).
What could be the reason for this?
I assume it's factory calibrated.
Here's the attached code with CC1310(CCS):
txBuffer[0] = 0x0C;
i2cTransaction.slaveAddress = 0x19;
i2cTransaction.writeBuf = txBuffer;
i2cTransaction.writeCount =1;
i2cTransaction.readBuf = rxBuffer;
i2cTransaction.readCount = 2;
status = I2C_transfer(i2c, &i2cTransaction);
while (status == false) {
// Unsuccessful I2C transfer
Display_printf(display, 0, 0, "Unsucessful I2C Read");
sleep(2);
}
txBuffer[0] = 0x28;
i2cTransaction.slaveAddress = 0x19;
i2cTransaction.writeBuf = txBuffer;
i2cTransaction.writeCount =1;
i2cTransaction.readBuf = rxBuffer;
i2cTransaction.readCount = 6;
status = I2C_transfer(i2c, &i2cTransaction);
while (status == false) {
// Unsuccessful I2C transfer
Display_printf(display, 0, 0, "Unsucessful I2C Read");
sleep(2);
}
/* Take 20 samples and print them out onto the console */
for (sample = 0; sample < 1231150; sample++) {
if (I2C_transfer(i2c, &i2cTransaction)) {
/* Extract degrees C from the received data; see TMP116 datasheet */
//temperature = (rxBuffer[0] << 😎 | (rxBuffer[1]);
//temperature *= 0.0078125;
TMP = (rxBuffer[0] <<8) | (rxBuffer[1]);
AcX = (rxBuffer[1] <<8) | (rxBuffer[2]);
AcY = (rxBuffer[3] <<8) | (rxBuffer[4]);
AcZ = (rxBuffer[5] <<8) | (rxBuffer[6]);
2019-05-22 03:25 AM
Hi, to check the I2C communication did you try a single read of the WHO_AM_I (0Fh) reg? You should get 33h value. Consider that the factory calibration are stored in the reserved registers 00h-06h and could be 00h. Another point is if you are using the I2C multi-read sequence according to ds specs? Its very strange you see only one axis well (maybe only MSByte)... Better if it is possible for you to share the oscilloscope screenshots. Regards.
2019-05-22 04:44 AM
Hi, Thanks for your quick reply. I tried reading the OFh Register But as you can see it's returning 51(integer).
Since I don't have an oscilloscope, I'll check and share you the screenshots shortly.
2019-05-22 04:45 AM
and with this code:
txBuffer[0]=0x0F;
i2cTransaction.slaveAddress = 0x19;
i2cTransaction.writeBuf = NULL;
i2cTransaction.writeCount = 0;
i2cTransaction.readBuf = rxBuffer;
i2cTransaction.readCount = 2;
status = I2C_transfer(i2c, &i2cTransaction);
if (!status) {
// Unsuccessful I2C transfer
}
txBuffer[1] = 0x0C;
//txBuffer[1] = 0;
i2cTransaction.slaveAddress = 0x19;
i2cTransaction.writeBuf = txBuffer;
i2cTransaction.writeCount =1;
i2cTransaction.readBuf = rxBuffer;
i2cTransaction.readCount = 2;
status = I2C_transfer(i2c, &i2cTransaction);
while (status == false) {
// Unsuccessful I2C transfer
Display_printf(display, 0, 0, "Unsucessful I2C Read");
sleep(2);
}
//txBuffer[0] = 0x3B;
txBuffer[2] = 0x28;
i2cTransaction.slaveAddress = 0x19;
i2cTransaction.writeBuf = txBuffer;
i2cTransaction.writeCount =1;
i2cTransaction.readBuf = rxBuffer;
i2cTransaction.readCount = 6;
status = I2C_transfer(i2c, &i2cTransaction);
while (status == false) {
// Unsuccessful I2C transfer
Display_printf(display, 0, 0, "Unsucessful I2C Read");
sleep(2);
}
/* Take 20 samples and print them out onto the console */
for (sample = 0; sample < 1231150; sample++) {
if (I2C_transfer(i2c, &i2cTransaction)) {
/* Extract degrees C from the received data; see TMP116 datasheet */
//temperature = (rxBuffer[0] << 😎 | (rxBuffer[1]);
//temperature *= 0.0078125;
whoami= (rxBuffer[0]) | (rxBuffer[1]);
TMP = (rxBuffer[2] <<8) | (rxBuffer[3]);
AcX = (rxBuffer[4] <<8) | (rxBuffer[5]);
AcY = (rxBuffer[6] <<8) | (rxBuffer[7]);
AcZ = (rxBuffer[8] <<8) | (rxBuffer[9]);
Temperature =TMP/340.00+36.53
2019-05-27 01:51 AM
Did you correctly initialize the reg CTRL_REG1 (20h) in terms of ODR value? Lçet me pls know if you succeed in correctly reading the data. Regards
2019-05-28 04:00 AM
Yea I have set CTRL_REG1(20h) to 57h i.e. 0101 (100Hz ODR) but still Accel x,y,z, values never changes.
Code:
/*
* ======== i2ctmp116.c ========
#include <stdint.h>
#include <stddef.h>
#include <unistd.h>
/* Driver Header files */
#include <ti/drivers/GPIO.h>
#include <ti/drivers/I2C.h>
#include <ti/display/Display.h>
#include <xdc/runtime/System.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/PIN.h>
/* Example/Board Header files */
#include "Board.h"
#define TASKSTACKSIZE 640
#define LIS_2DH 0x0000
#ifdef Board_I2C_LIS_ADDR
#define LIS_2DH_ADDR Board_I2C_LIS_2DH_ADDR
#else
#define LIS_2DH_ADDR 0x19 //0x18 AD=1
#endif
static Display_Handle display;
/*
* ======== mainThread ========
*/
char tmp_str[7]; // temporary variable used in convert function
char* convert_int16_to_str(int16_t i) { // converts int16 to string. Moreover, resulting strings will have the same length in the debug monitor.
printf(tmp_str, "%6d", i);
return tmp_str;
}
void myCallbackFxn(I2C_Handle handle, I2C_Transaction *msg, bool status)
{
if (status == false) {
//transfer failed
}
}
void *mainThread(void *arg0)
{
void taskFunction(); {
uint16_t sample;
uint8_t AcX,AcY, AcZ,who_am_i,control1,TMP_CFG,CTRL_REG1;
uint8_t TMPH,TMPL;
// uint16_t xAccel,yAccel,zAccel;
int16_t TMP;
float Temperature;
uint8_t txBuffer[3];
uint8_t rxBuffer[9];
//uint16_t Ax,Ay,Az;
bool status;
//I2C_Handle i2cHandle = I2C_open(Board_I2C_GY521_MPU6050, &i2cParams);
//I2C_Handle i2c;
I2C_Params i2cParams;
I2C_Params_init(&i2cParams);
//i2cParams.transferMode = I2C_MODE_CALLBACK;
i2cParams.transferMode = I2C_MODE_BLOCKING;
i2cParams.transferCallbackFxn = myCallbackFxn;
i2cParams.bitRate = I2C_100kHz;
//I2C_Transaction i2cTransaction;
//I2C_Handle i2c = I2C_open(Board_I2C0, &i2cParams);
I2C_Handle i2c = I2C_open( Board_I2C_LIS, &i2cParams);
I2C_Transaction i2cTransaction = {0};
/* Call driver init functions */
Display_init();
GPIO_init();
I2C_init();
/* Configure the LED and if applicable, the TMP116_EN pin
GPIO_setConfig(Board_GPIO_LED0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
#ifdef Board_GPIO_TMP116_EN
GPIO_setConfig(Board_GPIO_TMP116_EN, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_HIGH);
/* 1.5 ms reset time for the TMP116
sleep(1);
#endif */
/* Open the HOST display for output */
display = Display_open(Display_Type_UART, NULL);
if (display == NULL) {
while (1);
}
/* Turn on user LED */
//GPIO_write(Board_GPIO_LED0, Board_GPIO_LED_ON);
//Display_printf(display, 0, 0, "Starting the i2ctmp116 example\n");
Display_printf(display, 0, 0, "Starting the LIS2DH-Accelerometer example\n");
/* Create I2C for usage */
I2C_Params_init(&i2cParams);
i2cParams.bitRate = I2C_400kHz;
//i2c = I2C_open(Board_I2C_TMP, &i2cParams);
i2c = I2C_open(Board_I2C_LIS, &i2cParams);
//i2c = I2C_open(CC1310_LAUNCHXL_I2C0_SDA0, &i2cParams);
//i2c = I2C_open(CC1310_LAUNCHXL_I2C0_SCL0 , &i2cParams);
if (i2c == NULL) {
Display_printf(display, 0, 0, "Error Initializing I2C\n");
while (1);
}
else {
Display_printf(display, 0, 0, "I2C Initialized!\n");
}
/* Who_am_i */
txBuffer[0] = 0x0F; //Who_am_i register = 0x0Fh 8 bit
i2cTransaction.slaveAddress = 0x19;
i2cTransaction.writeBuf = txBuffer;
i2cTransaction.writeCount = 1;
i2cTransaction.readBuf = rxBuffer;
i2cTransaction.readCount = 1;
/* CTRL_REG1 = 20h and Value is 57h */
txBuffer[1] = 0x20;
txBuffer[2] = 0x57;
i2cTransaction.slaveAddress = 0x19;
i2cTransaction.writeBuf = txBuffer;
i2cTransaction.writeCount = 2;
i2cTransaction.readBuf = rxBuffer;
i2cTransaction.readCount = 1;
/* Accelerometer values x,y & z */
txBuffer[4] = 0x28;
i2cTransaction.slaveAddress = 0x19;
i2cTransaction.writeBuf = txBuffer;
i2cTransaction.writeCount =1;
i2cTransaction.readBuf = rxBuffer;
i2cTransaction.readCount = 6;
status = I2C_transfer(i2c, &i2cTransaction);
while (status == false) {
// Unsuccessful I2C transfer
Display_printf(display, 0, 0, "Unsucessful I2C Read");
sleep(2);
}
/* Take 20 samples and print them out onto the console */
for (sample = 0; sample < 1231150; sample++) {
if (I2C_transfer(i2c, &i2cTransaction)) {
who_am_i = rxBuffer[0];
CTRL_REG1 = rxBuffer[1];
AcX =(rxBuffer[2] <<8) | (rxBuffer[3]);
AcX =(rxBuffer[4] <<8) | (rxBuffer[5]);
AcX =(rxBuffer[6] <<8) | (rxBuffer[7]);
Display_printf(display, 0, 0,"who_am_i is: %d \n", who_am_i);
Display_printf(display, 0, 0,"CTRL_REG1 is: %d \n", CTRL_REG1);
Display_printf(display, 0, 0, "AcX is : %d \t rxBuffer[3] : %d \t rxBuffer[2] : %d \n", AcX,rxBuffer[2], rxBuffer[3]);
Display_printf(display, 0, 0, "AcY is : %d \t rxBuffer[5] : %d \t rxBuffer[4] : %d \n", AcY,rxBuffer[4], rxBuffer[5]);
Display_printf(display, 0, 0, "AcZ is : %d \t rxBuffer[7] : %d \t rxBuffer[6] : %d \n", AcZ,rxBuffer[6], rxBuffer[7]);
}