cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H750 system boot loader via CAN?

MMagl
Associate III
Error while parsing Rich Text Content
1 ACCEPTED SOLUTION

Accepted Solutions
Amel NASRI
ST Employee

Hi @MMagl​ ,

I am coming back to answer your question.

The current STM32H7 bootloader doesn't support CAN interface. The AN2606 is the reference and is the correct one.

However, for STM32H7 rev V devices, the FDCAN bootloader interface will be supported.

AN2606, AN4938 and AN3154 will be updated accordingly.

-AMel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
MMagl
Associate III

It seems that STM forum have some restriction for text formatting and I end-up with strange post. Here is my second attempt.

Can I perform boot via CAN interface using the STM32H750 boot loader?

  1. Old version of AN2606 says that it deppen on bool loader version. Version xx does not support and version yy has CAN support with some limitations.
  2. The newest AN2606 from February 2019 says that there is no support for CAN boot – AN2606 page 193-198

https://www.st.com/content/ccc/resource/technical/document/application_note/b9/9b/16/3a/12/1e/40/0c/CD00167594.pdf/files/CD00167594.pdf/jcr:content/translations/en.CD00167594.pdf

According to AN4938 page 24 chapter 5.3 says that CAN2 PB5/PB13 can be used for boot.

https://www.st.com/content/ccc/resource/technical/document/application_note/group0/e8/d8/d0/32/33/94/41/dd/DM00337873/files/DM00337873.pdf/jcr:content/translations/en.DM00337873.pdf

That is why I asking this question

Thanks in advance

Amel NASRI
ST Employee

Hi @MMagl​ ,

I am coming back to answer your question.

The current STM32H7 bootloader doesn't support CAN interface. The AN2606 is the reference and is the correct one.

However, for STM32H7 rev V devices, the FDCAN bootloader interface will be supported.

AN2606, AN4938 and AN3154 will be updated accordingly.

-AMel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

MMagl
Associate III

Thanks for clarification

The message thread can be put to solved state

Thanks,

Mirtcho