cancel
Showing results for 
Search instead for 
Did you mean: 

STM32769 Disco not working with TouchGFX and CubeMX

Hello

I am using the STM32F769-Disco Board with Touchgfx and CubeMX (and Atollic True Studio). I am not getting it working with the following manual: https://touchgfx.zendesk.com/hc/en-us/articles/360020208091-Configuring-STM32F769I-DISCO

Can someone help me?

I've got the STM32F746-Disco running with parallel-RGB interface. The STM32769-Disco has a DSI interface and I do not know what I've done wrong or if the manual has some issues.

Dejan

2 REPLIES 2
Mon2
Senior III

Hi. Have not tested this target yet but the above referenced article details a procedure using the IAR compiler.

Are you using the IAR compiler?​

I am using Atollic True Studio.

When I am setting up the project with STM32CubeMX then I can't get the display working with TouchGFX.