2019-04-15 03:15 PM
I'm building a CAN app with STM32CUBEMX and TrueStudio. I'm using interrupts so need to register my calback funcs. I put #define USE_HAL_CAN_REGISTER_CALLBACKS 1 at the top of main.h. The following line in my code:
HAL_CAN_RegisterCallback(&hcan1, HAL_CAN_RX_FIFO0_MSG_PENDING_CB_ID, HAL_CAN_RxFIFO0MsgPendingCallback );
is producing the error "HAL_CAN_RX_FIFO0_MSG_PENDING_CB_ID undeclared". But it is a value of the enum type HAL_CAN_CallbackIDTypeDef which is declared in stm32f4xx_hal_can.h which is included in main.h. I'm stumped.
Solved! Go to Solution.
2019-04-15 04:05 PM
2019-04-15 04:05 PM
2019-04-15 05:34 PM
That worked, thanks. I was following instructions in stm32f4xx_hal_can.c which said I had to do all this register callbacks rigamarole. I took that all out and I'm at least compiling. Will test tomorrow.