cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F732 UART bootloader, with FLASH loader demostrator

ihouses ihouses
Associate III

Hello,

I want to use the STM32F732 bootloader with the UART. I am using the ST flash demostrator. I connect the UART by means of a USB to UART converter (SiLabs). The FLASH software ​finds something and says that the part is readable but is not possible to click 'remove protection' button. When I click next the target is empy and the list is also empy. Is it my chip supported by the Flash Loader demostrator? All the other features doesn't work either since looks like that the device is protected.

Is there any UART bootloader working with my part?

1 REPLY 1
ihouses ihouses
Associate III

Finally the problem is that Flash Loader demonstrator doesn't support the STM32F32xx devices (looks to me). I managed to implement in python a uart booloader code but when I do the verification I see that the flasher is actually not writing anything.

Is it possible that flash protection is activated and that is the problem? I am using System Workbench to generate the .BIN file and I use St Link V2. I was searching and I can not see where to enable/disable flash protection. Where is it??