cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F778, VDD 1.8V, USB not working

MVore
Associate II

We have a design using the STM32F778. The FS USB works fine with VDD = 3.3V. When VDD = 1.8V, the USB does not work. VDDUSB is connected to 3.3V in both cases. On some boards, the FS USB will be detected by PC as a bootloader but it does not actually work. Anyone have success with one of the STM32F7 parts USB when VDD = 1.8V?

5 REPLIES 5
Imen.D
ST Employee

Hello,

Check the condition in this datasheet relevant to your device.

Regards,

Imen.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
S.Ma
Principal

Check the power sequences to follow. Maybe the power up/down is wrong.

MVore
Associate II

The power sequence is compatible with what is in the datasheet.

Alex R
Senior

What is your max HCLK when using Vdd=1.8?

MVore
Associate II

180 MHz