cancel
Showing results for 
Search instead for 
Did you mean: 

the F302 project example of X-CUBE-SPN8 doesn't work

frank239955
Associate II

Dear

I try to flash the example image which is located at the following path

"STM32CubeExpansion_SPN8_V1.0.1\Projects\Multi\Examples\MotorControl\Src"

to development board and using six-step to start motor

but the motor doesn't startup , check the failure reason is startup failure

Doex enveryone knows how to run this example​?

thanks

I use

1. "nucleo f302r8" as the development board

2 "X-NUCLEO-IHM08M1" as the power board

3 " BR2804-1700Kv-1" as the motor

1 REPLY 1
DBake.18
Associate II

For six step control please check the next jumper settings:

  • JP1 open,
  • JP2 open
  • JP5 and JP6 on 1Sh position

All jumpers you can see on below picture (UM1943):

 0690X0000089yvqQAA.png

With above jumper settings, you make configuration for 1 shunt current reading (which is requested for six step motor control). You can find more information on L6230 datasheet.

0690X0000089yw0QAA.png

Kind regards,

Dražen