cancel
Showing results for 
Search instead for 
Did you mean: 

Enabling Internal RTC of the STM32F746G-DISCO in TouchGFX projects

Ameya M
Associate III

Hello,

I want to display the current time in TouchGFX project.

I am using TGFX 4.9.3 (using Keil IDE) and I want to use the Internal RTC to update set time.

The issue is that the clock settings are already defined when the project is created.

So I tried adding the required Clock Config (added in BoardConfiguration.cpp).

But it is not working.

Thanks,

Ameya

0 REPLIES 0