cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX v5.1.0 project generating error in mint linux(based on ubuntu).

SKIM.191
Associate

After project setting, I want to make this setting TrueStudio project.

So, I pushed generate code button, but it didn't work with error message pop up.

I already installed the jre, jdk.

How can I solve this problem?

What is the ProjectBuilder below?

2019-03-25 15:13:30,303 [INFO] ConfigFileManager:1281 - mx.scratch is deleted!

2019-03-25 15:13:30,303 [INFO] ProjectBuilder:2035 - Time for Generating toolchain IDE Files: 17mS.

2019-03-25 15:13:30,304 [ERROR] ProjectBuilder:2041 - Error in Project Generation

2019-03-25 15:13:30,304 [ERROR] ProjectBuilder:588 - Error in Project Generation

0 REPLIES 0