cancel
Showing results for 
Search instead for 
Did you mean: 

Doubts about AN4013 and timer gated mode

Uwe Bonnes
Principal II

Hello,

an4013 Rev. 6 on page 21 writes:

"The Counter Enable signal is generated by a logic OR between CEN control bit and the trigger input when configured in gated mode."

while e.g. RM0351 writes:

"Enable the counter by writing CEN=1 in the TIMx_CR1 register (in gated mode, the

 counter doesn't start if CEN=0, whatever is the trigger input level)."

This contradicts and probably AN4013 is wrong and should read "logic AND"

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @Uwe Bonnes​ ,

You are right, I confirm that the AN4013 is wrong. This sentence will be fixed in the next revision Rev7 which is about to be published in a few weeks.

Thanks again for pointing this error out.

Regards,

-Imen-

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

1 REPLY 1
Imen.D
ST Employee

Hello @Uwe Bonnes​ ,

You are right, I confirm that the AN4013 is wrong. This sentence will be fixed in the next revision Rev7 which is about to be published in a few weeks.

Thanks again for pointing this error out.

Regards,

-Imen-

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen