cancel
Showing results for 
Search instead for 
Did you mean: 

How can i avoid the emptying of flash ID file when re-generating code from CubeMX?

vicfer89
Associate II

At the time I re-generates the code in CubeMX, the Flash ID file is emptied and i have to copy it from a previous version or a copy out of my code directory.

The first time that the code is generated it works properly, and it can be compiled as usually.

I'm loading the basic CubeMX configuration for NUCLEO-144 STM32F746ZG with LWIP libraries activated, and Eclipse IDE for C/C++ Developers Version: 2018-12 (4.10.0) with the latest revision of AC6 system workbench.

I'm using latest version (V 5.1.0) of CubeMX to generate my code.

Thanks in advance for your response and support.

0 REPLIES 0