cancel
Showing results for 
Search instead for 
Did you mean: 

How to configure ST25DV registers via I2C

Central SUPPORT
Senior II

I have a question for the configuration of the static registers via the I2C bus.

The easiest way to configure the Area RF protection and Area ending point registers, (address 0x0004 until 0x000A), is to send a I2C write message to program all 7 data bytes in one I2

See the table 11 snapshot from the datasheet:

0690X000006DvcFQAS.png

However, data is not programmed. Any suggestion why it does not work?

NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.

1 ACCEPTED SOLUTION

Accepted Solutions
Central SUPPORT
Senior II

In fact, configuration registers must be programmed byte-by-byte in separate I2C Write Byte command messages.

We recommend to                                       

·       first set the area limit registers (ENDA1, ENDA2, ENDA3) and

·       then set RF security status registers (RFAnSS).

View solution in original post

1 REPLY 1
Central SUPPORT
Senior II

In fact, configuration registers must be programmed byte-by-byte in separate I2C Write Byte command messages.

We recommend to                                       

·       first set the area limit registers (ENDA1, ENDA2, ENDA3) and

·       then set RF security status registers (RFAnSS).