cancel
Showing results for 
Search instead for 
Did you mean: 

Does TouchGfx currently has support for i.MX6 UL board? I need to develop application screen which has to be run on imx6ul board.

pmv
Associate
 
2 REPLIES 2
Mon2
Senior III

No. Do not believe so. TouchGFX (formerly Draupner product and now owned by ST) is strictly for the STM32 CPU targets.

Martin KJELDSEN
Chief III

Hi @pmv​,

Besides the truths that @Mon2​ are posting, I thought i'd just add something to this.

TouchGFX 4.10.0 and onwards are STM32 locked. Prior to that, they're not. That being said, the port for IMX6UL was always unofficial and just something i had running at my desk running Yocto Linux, so you won't find any support through the designer even if you're using an old version.

Best regards,

Martin