cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-NFC03A1 plugged on top of NUCLEO-L476RG example

LGrig
Associate

I am trying to read nfc cards with X-NUCLEO-NFC03A1 plugged on top of NUCLEO-L476RG. However, in the X-CUBE-NFC3 ver. 1.4.0 there is no example for such combination, but according to UM2045 Rev 2 ("The software comes with examples of implementation of such drivers, running on X-NUCLEO-NFC03A1 plugged on top of one NUCLEO-L476RG, NUCLEO-F401RE or NUCLEO-F103RB. ") somewhere should be such an example.

Could you please point out exactly where this example project can be downloaded?

Thanks in advance!

Linards

1 ACCEPTED SOLUTION

Accepted Solutions
Rene Lenerve
ST Employee

Hi @LGrig​ ,

Yes you are right, the documentation is indicating the L4 platform, but it is not present in the software package, this is a mistake. Please have a look to the following thread https://community.st.com/s/question/0D50X00009sUl5WSAS/read-the-rfid-of-a-card-with-nfc03a1, I've already made the porting to this platform for someone.

Let me know if that helps you.

Regards.

View solution in original post

1 REPLY 1
Rene Lenerve
ST Employee

Hi @LGrig​ ,

Yes you are right, the documentation is indicating the L4 platform, but it is not present in the software package, this is a mistake. Please have a look to the following thread https://community.st.com/s/question/0D50X00009sUl5WSAS/read-the-rfid-of-a-card-with-nfc03a1, I've already made the porting to this platform for someone.

Let me know if that helps you.

Regards.