cancel
Showing results for 
Search instead for 
Did you mean: 

RM0395, STM32L412 and ADC12_CLK

Uwe Bonnes
Principal II

Hello,

RM0394 Rev. 4 chapter 16.4.2 clocks should note in a preamble or something similar that Dual clock and ADC12_CLK is not available on STM32L412. Reading through RM0394 I conclude that ADC clock is HCLK fixed on L412, but I don't see it stated anywhere. If the description in 6.4.27 for Bits 28/29 whould state the ADC Clock for STM32L412 is HCLK fixed, thing would be clearer.

Kind regards

1 ACCEPTED SOLUTION

Accepted Solutions
Viktor POHORELY
ST Employee

Thank you to point this out, in next revision of RM0394, note linked to bits 28/29 will highlight this fact to be more clear.

View solution in original post

3 REPLIES 3
Viktor POHORELY
ST Employee

Thank you to point this out, in next revision of RM0394, note linked to bits 28/29 will highlight this fact to be more clear.

@Uwe Bonnes​  , maybe you want also to fix the number of RM in the title, so that it could be easier to look up this post when needed (also in the other thread you posted yesterday).

Jan

Uwe Bonnes
Principal II

How can I change the title?