2019-02-04 09:29 AM
I have a LSM6DSO and I want to test it with the data ready interrupt, but I don't get any. I am using a logic analyzer to monitor the interrupt.
The registers that I set are:
0x18 with value 0x01
0x0B with value 0x01
0x10 with value 0x40
0x0D with value 0x01
I am also reading the accelerometer registers in while(1) and it is working ok, but I have no interrupt. Should I set anything else?
Thanks,
Gabriel
2019-02-05 03:14 AM
Solved! I wrote a wrong value to a register 🙂