2019-01-30 04:56 AM
Hello,
I am using the STM32H743I-EVAL and have developed an application with GUI, using the built-in display MB1063 Rev.B.
In order to make a product from the application, I need a stock if working displays.
The built-in display is manufactured by Ampire, and its part number is
AM640480G5TNQW-T00H. I tried to contact this company at least 3 times but they did not reply.
Can anyone recommend me of other displays that could be connected to the STM32H743I-EVAL? Are there any other plug-and-play LCDs for this evaluation module? I prefer a TFT with higher resolution (800X600 or 1024X768 or higher), but the display external size can be even smaller.
Thanks.
Sagiftw
2019-04-16 07:58 AM
It is very weired that until now, April 16'th, no one answered to this post...
Does it mean that no one is using this CPU with TFT display?
2019-04-16 08:29 AM
2019-04-16 08:41 AM
They are busy for 2.5 months? And I am not so busy to your opinion?
Besides that, the STM32H743 does not support a DSI display (MIPI interface).