cancel
Showing results for 
Search instead for 
Did you mean: 

How to map PA2 to Nucleo CN10:37?

I'm unable to successfully see my PWM signal on the Nucleo STM32F302R8 development board, connector 10, pin 37.

I have SB62 and SB59 connected with 0-ohm resistors. I don't understand why the same pin is on multiple pins. Absolute pin number 17 AND 18.

https://www.st.com/en/evaluation-tools/nucleo-f302r8.html

https://www.st.com/resource/en/schematic_pack/nucleo_64pins_sch.zip

Which solder bridges should I short?

1 REPLY 1

Because the pins/functions are limited. PA2 is used for the VCP USART as well as the Arduino serial.

PA2 is CN10.35

PA3 is CN10.37

REMOVE SB13 (PA2) and SB14,SB58,SB53,SB62 (PA3)

MAKE SB63 (PA2) and SB59 (PA3)

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..