2019-01-17 12:42 PM
Hello,
I would like to ask you a question. I would like to use the LPS33HW in my application with I2C bus, before I move with the software development I would like to check if the sensor works with given ambient conditions. I thought that it will be great if I can reuse the STEVAL-MKI109V3 board and the GUI to read the data. Unfortunately I cannot connect with the sensor if I am do it like on schematic ( see attach ). Could you be so kind and help me to understand what I should do in order to verify if the sensor sense 🙂
Thank you in advance
Jacek Pieczaba
2019-01-17 11:57 PM
> Unfortunately I cannot connect with the sensor if I am do it like on schematic ( see attach ).
What exactly is the problem ?
You will need pull-up resistors for I2C to work. There are none in the schematics.
2019-01-18 12:48 AM
@Community member the pull-up resistors are on the STEVAL-MKI109V3
@Jacek Pieczaba What is the error message you get from Unico? Do you have the latest version of the firmware in the STEVAL-MKI109V3?
2019-01-18 05:40 AM
Hello,
Thank you very much for the suggestions what to check. In the mean time I was working on this problem with application engineer from ST and we figure out what to do in order to make it works. I just wanted to share the solution :
After this modification external boards with Sensor works very well under the GUI which is exactly what I wanted to obtain.
Thank you very much
Jacek Pieczaba
ps. Miroslav before I get an error ( see attached ) , version of Unico 7.0.0.0