cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with using internal opamp on the STM32L4

Scott Dev
Senior

Hi

I have been reading an ST presentation regarding using the internal opamp on a STM32L433. Am I reading it correctly, this saves in having to use an external opamp? I want to use it for as a follower for the analogue input. I am not sure I am reading this correctly, can I use the internal opamps as followers (or PGA) for any of the analogue inputs? If I am using multiple analogue input channels, do I have to configure it each time before sampling the required channel A/D channel (point it to the required A/D channel)?

Regards

Scott

3 REPLIES 3
Piranha
Chief II

No, that's not how it works. Look at RM0394 20.3.3 Signal routing.

Scott Dev
Senior

Looking at 20.3.3, am I right in thinking that one a/d can be used, channel 8? Any other channel I would need external opamp.

Regards

Scott

Piranha
Chief II

Yes, that's correct.