2018-12-11 02:29 PM
I need to store atleast 20,000 samples per second to perform FFT. so I have used memory card to store all the values in sd card. currently, I could only able to store 7000 samples at a particular interval of time but not more than that. I tried with one bit sdio mode and 4 bit but of no avail.
Any hints or tips to improve the speed of sdio mode? I also tried to increase the overall frequency of the clock then too it didnt affect the performance of sdio.
in the code for my trail purpose i simply created an array. In future I will store values from ADC inputs in array. when i change the value in array to 8000 and value in for loop to 7999 nothing happens! I could only able to create a .txt file in sd card but i cannot store values.
simple code:
uint16_t array[7000],j=1;
/* USER CODE BEGIN 2 */
if(f_mount(&myFatFS, SDPath,1) == FR_OK)
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET);
char myFILEName[]="TEST1.txt";
if(f_open(&myFILE, myFILEName, FA_WRITE| FA_CREATE_ALWAYS) == FR_OK)
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
for(int i=0; i<=6999; i++)
{
array[i]=j;
j++;
}
if(f_write(&myFILE, array, sizeof(array), &myBytes)==FR_OK)
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);
}
f_close(&myFILE);
}
}
Solved! Go to Solution.
2018-12-12 02:03 PM
Thanks for the inputs yes, there is a bug i found it! I declared local variable array for some reason it might be storing less amount of bytes when i declared globally it increased the total number of numbers to maximum space of microcontroller flash memory.
2018-12-11 02:55 PM
>> I could only able to create a .txt file in sd card but i cannot store values.
Variables store in binary are not going to display nicely in ASCII via TYPE or CAT type commands, or loading into a text editor.
Look at the data in a File Viewer or Hex Editor
Opening/Closing a file repeatedly will be slow.
The file system and card want stuff in powers of two, ie writes of 8192 bytes or 32768 bytes for instance.
2018-12-11 02:56 PM
2018-12-12 08:37 AM
Are there better alternatives to store numerical data other than .txt format ? If yes can you let me know please .I should be able to view the data in computer after storing.
Yes I am using hex editor to view the data.
I tried with 8192 size of array but for some reason it is not loading in data. I also tried with 32768 as well. one interesting thing is, when i kept the size of array 4096, the system didnt upload data to memory card but when i kept 5000 it worked. for array sizes: 4000,5000,6000,7000, the system worked but for more than 7000 size of array it didnt work !!!!!!
2018-12-12 09:09 AM
>>Are there better alternatives to store numerical data other than .txt format ?
You've given the file an arbitrary extension, you are writing binary data as 16-bit words to the file. The file in this context is a collection of bytes. It is not text or ASCII formatted.
>>I should be able to view the data in computer after storing.
View them as a human, or have an application read the structures and process as standard 16-bit representations?
If you want to import into Excel you might need a more verbose/human centric format like comma delimited ASCII fields (See .CSV)
Binary data is covered by Computers 101 Data Representation means/methods.
A functional file system shouldn't care if there are 7000 or 8192, suggests there are bugs in stack somewhere.
>>... size of array it didnt work !!!!!!
I don't know how to debug that, what did it actually write vs what was expected?
2018-12-12 02:03 PM
Thanks for the inputs yes, there is a bug i found it! I declared local variable array for some reason it might be storing less amount of bytes when i declared globally it increased the total number of numbers to maximum space of microcontroller flash memory.