cancel
Showing results for 
Search instead for 
Did you mean: 

touchGFX 4.10.0, Iar EWARM 8.3 User Bitmap image Error.

ikassma
Senior

@I use STM32F769I-DISCO Board. with IAR EWARM 8.3, TouchGFX 4.10.0

The output for the image I attached is not working properly.

I also have the STM32F746G-DISCO board and have the same symptoms.

I just compiled and tested the example project of TouchGFX in IAR8.3 without any modification.

IAR 8.3 compiler confirmed that STM32F746G-DISCO works fine in TouchGFX 4.9.3 and all examples in TouchGFX 4.10.0 do not work properly.

What should I do?

1 REPLY 1
Martin KJELDSEN
Chief III

Hi,

Are you using Application Templates from within the TouchGFX designer or did you use CubeMX to generate your projects? Also, could you post some error logs that show the problems you're having?

Thanks!