2018-11-26 02:16 AM
Hi Guys,
I created a Keil5 project with CubeMX. In this project, i only created a USART (USART1) periphery application. So simple as that. BUT: My usart seams not to run. I enabled it by "HAL_USART_ENABLE_IT" in the setup and call the "HAL_USART_RECEIVE_IT" in the USART1_IRQHandler function. Secondly i tried to enable RCC-Clock by "__HAL_RCC_USART1_CLK_ENABLE();", but my buffer was still empty.
In the Debug Session, i made a Screenshot of the huart1 variable. There you can see the values of every Register during debugging. They stay all the same, so no chasnges during debugging.
Do you see anything I missed for calling? The USART clock should be connected with the usart periphery automatically by using CubeMX, souldn't it?
Thank you and have a nice day.
2018-11-26 06:11 AM
Only seeing 3 files. ZIP up compilable projects don't attach multiple files.
Not sure what board or what pins are involved.
Check GPIO pins and clocks
Check HSE_VALUE define and PLL setting relative to chosen clock source/parts.
2018-11-26 07:22 AM
Hi, I already found the mistake, was a pure pin fault...
I'd like to explain my question as done, where do I do that?
2018-11-26 09:39 AM