cancel
Showing results for 
Search instead for 
Did you mean: 

SPC5 Flasher 2.7.1 usb to uart converter showed as hybrid only and can't connect anymore

aurelien23
Senior

With version 2.6.2b I was selecting my USB to serial converter using the "non hybrid" definition. Now with 2.7.1 I only see the "Hybrid" definition and it can't connect.

"[2018/11/16 15:21:17]: SPC5 Flash Programmer 2.7.1 - Start connection: Target:SPC564B74 - External crystal: 40MHz - Interface: UCUART::HybridCom/1/UART

[2018/11/16 15:21:20]: An error occured during plugin downloading via BAM/BAF

[2018/11/16 15:21:20]: Connection end.

"​

2 REPLIES 2
Erwan YVIN
ST Employee

Hello Aurelien ,

Do you use SPC564B74 Discovery or Minimodule ?

i am checking the issue

Best regards

Erwan

aurelien23
Senior
Hi Erwan,
I’m using a finished product I developed and I have to flash it in fields using a usb to serial converter. This one was only seen as hybrid in 2.7.1.
After reinstalling the old 2.6.2 I was fzcing the same issue and I solved it by deleting the SPC5 Flasher install folder after uninstall it and reinstalled it.
I did not try the same procedure with 2.7.1.
Hope it helps
Aurélien