2018-11-13 08:53 PM
Hi:
Let me ask you a question.
When use 32 bits of SDRAM in STM469 official routines, DMA is configured as follows:
/* Configure common DMA parameters */
dma_handle.Init.Channel = SDRAM_DMAx_CHANNEL;
dma_handle.Init.Direction = DMA_MEMORY_TO_MEMORY;
dma_handle.Init.PeriphInc = DMA_PINC_ENABLE;
dma_handle.Init.MemInc = DMA_MINC_ENABLE;
dma_handle.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
dma_handle.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
dma_handle.Init.Mode = DMA_NORMAL;
dma_handle.Init.Priority = DMA_PRIORITY_HIGH;
dma_handle.Init.FIFOMode = DMA_FIFOMODE_DISABLE;
dma_handle.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
dma_handle.Init.MemBurst = DMA_MBURST_SINGLE;
dma_handle.Init.PeriphBurst = DMA_PBURST_SINGLE;
dma_handle.Instance = SDRAM_DMAx_STREAM;
/* Associate the DMA handle */
__HAL_LINKDMA(hsdram, hdma, dma_handle);
/* Deinitialize the stream for new transfer */
HAL_DMA_DeInit(&dma_handle);
/* Configure the DMA stream */
HAL_DMA_Init(&dma_handle);
Now I change SDRAM to 16 bit data width. Should DMA also be modified accordingly? If so, how should it be modified in the configuration?
Thank you very much.
2018-11-13 09:14 PM
2018-11-13 10:14 PM
Because the data width of my product SDRAM is 16 bits. So I wonder if I want to change the data width of SDRAM dam to 16 bits.
2018-11-13 10:15 PM
Because the data width of my product SDRAM is 16 bits. So I wonder if I want to change the data width of SDRAM dam to 16 bits.