2018-11-12 02:25 AM
2018-11-12 02:55 AM
What bootloader addresses ?
For the system BL, no. And that's a good thing.
2018-11-12 08:54 AM
2018-11-14 03:11 AM
Which part is writable?
2018-11-14 03:15 AM
I want to change the start address of the main code and no one else can figure out the start address by reading the flash.How can I do such a thing?
2018-11-14 05:09 AM
The boot loader doesn't determine that. Assume your actual adversaries understand the platform/technologies better than you, they have more time and more resources. Figure you are matching wits with Einstein or Tesla, or both at once.
If the micro-controller can figure it out how hard can it be for anyone else?
Are you talking about your own loader, or the system loader (BOOT0=High)?
The memory at 0x1FFxxxxx other than the options and OTP is generally not writable.
On the H7 I think you can specify a start block for the vector table, but not sure how useful that is.