cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-ESC001V1 and Motor Control Workbench 5.2 - Image size exceeds the maximum allowed size

Amrit Singh
Associate II

When I use the motor control workbench with KEIL uvision 5.25, I get the following error:

linking...

ESC001\ESC001.axf: error: L6047U: The size of this image (33032 bytes) exceeds the maximum allowed for this version of the linker

Finished: 0 information, 0 warning, 0 error and 1 fatal error messages.

"ESC001\ESC001.axf" - 1 Error(s), 0 Warning(s).

Target not created.

I read somewhere that there are compiler options to reduce code size - which were for AC6. Can anyone guide me towards fixing these errors for uVision.

Thanks!

1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards