cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to connect the exposed pad to Vss in a VFQFPN36 STM32F103T8U?

RMele
Associate II

It's possible connect the exposed pad to Vss in a VFQFPN36 STM32F103T8U? What happen if I do it?

In the datasheet STM say about UFQFPN48 "It is recommended to connect it to VSS", but say nothing about about the VFQFPN36 package

5 REPLIES 5
Uwe Bonnes
Principal II

This is clearly missing from the datasheet. I guess, the exposed pin on VFQFPN36 will behave like on UFQFPN48, but some feedback from ST would clear up things.

T J
Lead

if you could check the ePad with a multimeter to the ground pin on the processor...

either way, connected or not...

Yes , you can connect the ePad to Gnd.

provisos:

IMHO

not an ST employee

please check it works, before you make many units...

Amel NASRI
ST Employee

Hello,

Sorry for the delay to answer your request.

I confirm that it is recommended to connect the exposed pad of VFQFPN36 STM32F103T8U to VSS.

A note will be added to the relevant datasheet to bring more precision (wait for next revision of the document to add it).

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

​Thank you Amel!!!. I have 300 boards with the exposed pad connected to Vss, and I was fear to go into production.

RMele
Associate II

​Thank you TJ!