cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-MKI015V1 with STEVAL-MKI109V3 and Unico 7.0.0.0

SROSS
Associate

I'm trying to evaluate STEVAL-MKI015V1 with STEVAL-MKI109V3 and Unico 7.0.0.0. The device appears in the selection menu, but I got the error "Device is not supported by the motherboard". I successfully completed the firmware upgrade through DFU (current version is V2.30.3) and I'm able to evaluate other devices (i.e. STEVAL-MKI186V1 works fine). Is the device supported? Is there any specific hardware configuration I have to setup on the motherboard jumpers for analog accelerometer?

1 REPLY 1
Miroslav BATEK
ST Employee

STEVAL-MKI015V1 is not supported by the FW in STEVAL-MKI109V3.