cancel
Showing results for 
Search instead for 
Did you mean: 

Dual-image FW upgrade using serial stand-alone flash

Mikhail Soloviev
Associate

Hi everybody,

I wonder if it is possible to configure the X-CUBE-SBSFU expansion to use external serial flash chip instead of internal memory. Any ideas, application note?

regards

Mikhail

1 REPLY 1
ADach
Associate

Hi,

I'm actually working on the same topic. Actually, this is possible to download the new firmware image in external flash memory but you have to keep slot 0 in internal flash to be able to execute it.

Regards