cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-144 (stm32f767). USB FS. Changing pins DP, DM from PA11, PA12, to PB14, PB15 doesn't work.

NikDobro
Associate II

Hi, collegs!

I have NUCLEO-144 (STM32F767) board. I started USB-HID example. It worked. Then I have change in "HAL_PCD_MspInit" function pins from pins DP, DM from PA11, PA12, to PB14, PB15.

On my own board with STM32F767 USB is connected to this pins.

I just want to see, that DP pin is pulled up after initialization and usb start (without V power detection).

So, I was very wounder! After changes, initialization and usb start. The pin PA12 (DP) is pulled up!!! And pin PB15 isn't!

I have no idea why it works so...

In datasheet PA11 (OTG_FS_DM), PA12 (OTG_FS_DP), PB14 (OTG_HS_DM), PB15 (OTG_HS_DP).

May be the problem is in that difference FS (Pins A), HS (Pins B)?

I have change only "HAL_PCD_MspInit" function.

void HAL_PCD_MspInit(PCD_HandleTypeDef *hpcd)
{
  GPIO_InitTypeDef  GPIO_InitStruct;
  
  /* Configure USB FS GPIOs */
//  __HAL_RCC_GPIOA_CLK_ENABLE();
  
//  /* Configure DM DP Pins */
//  GPIO_InitStruct.Pin = (GPIO_PIN_11 | GPIO_PIN_12);
//  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
//  GPIO_InitStruct.Pull = GPIO_NOPULL;
//  GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
//  GPIO_InitStruct.Alternate = GPIO_AF10_OTG_FS;
//  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); 
 
  __HAL_RCC_GPIOB_CLK_ENABLE();
 
/* Configure DM DP Pins */
  GPIO_InitStruct.Pin = (GPIO_PIN_14 | GPIO_PIN_15);
  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
  GPIO_InitStruct.Alternate = GPIO_AF12_OTG_HS_FS;
  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); 
  
  /* Enable USB FS Clocks */
  __HAL_RCC_USB_OTG_FS_CLK_ENABLE();
  
  /* Set USBFS Interrupt priority */
  HAL_NVIC_SetPriority(OTG_FS_IRQn, 5, 0);
  
  /* Enable USBFS Interrupt */
  HAL_NVIC_EnableIRQ(OTG_FS_IRQn);
}

Can anybody help me? Why I have no DP up signal after usb start.

1 ACCEPTED SOLUTION

Accepted Solutions

>>May be the problem is in that difference FS (Pins A), HS (Pins B)?

Well they are two entirely separate controllers, so you'd need to carry that through the code completely.

It is referred to as HS_FS because it is capable of doing both modes, on its pins, not on the pins of both controllers.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2

>>May be the problem is in that difference FS (Pins A), HS (Pins B)?

Well they are two entirely separate controllers, so you'd need to carry that through the code completely.

It is referred to as HS_FS because it is capable of doing both modes, on its pins, not on the pins of both controllers.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
NikDobro
Associate II

Yeap! That was a good point!

I've change

  1. the "instance" in usb handle type structure to "USB_OTG_HS";
  2. Enable USB HS Clocks in "HAL_PCD_MspInit" function.

And it works! Now I have PA12 not working and PB15 is working. So what I wanted.

Thanks!

USBD_StatusTypeDef USBD_LL_Init(USBD_HandleTypeDef *pdev)
{
  /* Set LL Driver parameters */
  hpcd.Instance = USB_OTG_HS;
  hpcd.Init.dev_endpoints = 4;
  hpcd.Init.use_dedicated_ep1 = 0;
  hpcd.Init.ep0_mps = 0x40;
  hpcd.Init.dma_enable = 0;
  hpcd.Init.low_power_enable = 1;
  hpcd.Init.phy_itface = PCD_PHY_EMBEDDED;
  hpcd.Init.Sof_enable = 0;
  hpcd.Init.speed = PCD_SPEED_FULL;
  hpcd.Init.vbus_sensing_enable = 0;
  hpcd.Init.lpm_enable = 0;
  
  /* Link The driver to the stack */
  hpcd.pData = pdev;
  pdev->pData = &hpcd;
  
  /* Initialize LL Driver */
  HAL_PCD_Init(&hpcd);
  
  HAL_PCDEx_SetRxFiFo(&hpcd, 0x80);
  HAL_PCDEx_SetTxFiFo(&hpcd, 0, 0x40);
  HAL_PCDEx_SetTxFiFo(&hpcd, 1, 0x80);
  
  return USBD_OK;
}
 
void HAL_PCD_MspInit(PCD_HandleTypeDef *hpcd)
{
  GPIO_InitTypeDef  GPIO_InitStruct;
  
  /* Configure USB FS GPIOs */
//  __HAL_RCC_GPIOA_CLK_ENABLE();
  
//  /* Configure DM DP Pins */
//  GPIO_InitStruct.Pin = (GPIO_PIN_11 | GPIO_PIN_12);
//  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
//  GPIO_InitStruct.Pull = GPIO_NOPULL;
//  GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
//  GPIO_InitStruct.Alternate = GPIO_AF10_OTG_FS;
//  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); 
 
  __HAL_RCC_GPIOB_CLK_ENABLE();
 
/* Configure DM DP Pins */
  GPIO_InitStruct.Pin = (GPIO_PIN_14 | GPIO_PIN_15);
  GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
  GPIO_InitStruct.Alternate = GPIO_AF12_OTG_HS_FS;
  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); 
  
  /* Enable USB HS Clocks */
  __HAL_RCC_USB_OTG_HS_CLK_ENABLE();
  
  /* Set USBFS Interrupt priority */
  HAL_NVIC_SetPriority(OTG_FS_IRQn, 5, 0);
  
  /* Enable USBFS Interrupt */
  HAL_NVIC_EnableIRQ(OTG_FS_IRQn);
}