cancel
Showing results for 
Search instead for 
Did you mean: 

Zero-g level offset of LIS2DH12 at FS bit set to '11', and Normal resolution mode.

t.saito
Associate II

LIS2DH12, Zero-g level offset is 40mg at FS bit set to '00'.

When using the FS bit set to '11' and Normal resolution mode, what value is it?

40mg * 12 = 480mg ?

or

40mg * 48 = 1920mg?

1 ACCEPTED SOLUTION

Accepted Solutions
Miroslav BATEK
ST Employee

ST doesn't specify this value.

But I would expect that if the zero-g level at FS=2g is typically 40mg, for FS=16g it could be 8-times higher.

View solution in original post

4 REPLIES 4
Miroslav BATEK
ST Employee

ST doesn't specify this value.

But I would expect that if the zero-g level at FS=2g is typically 40mg, for FS=16g it could be 8-times higher.

t.saito
Associate II

Dear Miroslav BATEK,

Thank you for your reply.

But, I don't understand if zero-g level offset is affected by resolution mode(High resolution or Normal or Low-power).

Do not I have to worry about the resolution mode?

Miroslav BATEK
ST Employee

I don't think the resolution will have significant impact on the zero-g level.

t.saito
Associate II

Dear Miroslav BATEK.

Thank you!

Your answer was very helpful.