2018-10-09 11:14 AM
Hello,
I am attempting to integrate the X-CUBE-NFC5 package with an existing project using a STM32F469II MCU and IAR. I have imported and setup the directories exactly as the example project , excluding the application files; however, I am receiving a significant amount of errors and I am at a loss on how to resolve the issues. I was able to successfully build the example project provided with the package for the STM32F401RE-Nucleo board.
The main issue is with the rfalIsoDepInfo struct and the rfalBitRate enum in "rfal_isoDep.h"
/*! RFAL Bit rates */
typedef enum {
RFAL_BR_106 = 0, /*!< Bit Rate 106 kbit/s (fc/128) */
RFAL_BR_212 = 1, /*!< Bit Rate 212 kbit/s (fc/64) */
RFAL_BR_424 = 2, /*!< Bit Rate 424 kbit/s (fc/32) */
RFAL_BR_848 = 3, /*!< Bit Rate 848 kbit/s (fc/16) */
RFAL_BR_1695 = 4, /*!< Bit Rate 1695 kbit/s (fc/8) */
RFAL_BR_3390 = 5, /*!< Bit Rate 3390 kbit/s (fc/4) */
RFAL_BR_6780 = 6, /*!< Bit Rate 6780 kbit/s (fc/2) */
RFAL_BR_52p97 = 0xEB, /*!< Bit Rate 52.97 kbit/s (fc/256) Fast Mode VICC->VCD */
RFAL_BR_26p48 = 0xEC, /*!< Bit Rate 26,48 kbit/s (fc/512) NFCV VICC->VCD & VCD->VICC 1of4 */
RFAL_BR_1p66 = 0xED, /*!< Bit Rate 1,66 kbit/s (fc/8192) NFCV VCD->VICC 1of256 */
RFAL_BR_KEEP = 0xFF /*!< Value indicating to keep the same previous bit rate */
} rfalBitRate;
typedef struct {
uint8_t FWI; /*!< Frame Waiting Integer */
uint32_t FWT; /*!< Frame Waiting Time (1/fc) */
uint32_t dFWT; /*!< Delta Frame Waiting Time (1/fc) */
uint32_t SFGI; /*!< Start-up Frame Guard time Integer */
uint32_t SFGT; /*!< Start-up Frame Guard Time (ms) */
uint8_t FSxI; /*!< Frame Size Device/Card Integer (FSDI or FSCI) */
uint16_t FSx; /*!< Frame Size Device/Card (FSD or FSC) */
uint32_t MBL; /*!< Maximum Buffer Length (optional for NFC-B) */
rfalBitRate DSI; ///////// First error here
rfalBitRate DRI; /*!< Bit Rate coding from Poller (PCD) to Listener (PICC) */
uint8_t DID; /*!< Device ID */
uint8_t ***; /*!< Node ADdress */
bool supDID; /*!< DID supported flag */
bool supNAD; /*!< *** supported flag */
bool supAdFt; /*!< Advanced Features supported flag */
} rfalIsoDepInfo;
Here are the compile errors in question. Path names are edited for brevity and privacy.
Error[Pe018]: expected a ")" D:\Project_Dir\Middlewares\ST\rfal\Inc\rfal_isoDep.h 278
Error[Pe079]: expected a type specifier D:\Project_Dir\Middlewares\ST\rfal\Inc\rfal_isoDep.h 278
Error[Pe168]: a function type is not allowed here D:\Project_Dir\Middlewares\ST\rfal\Inc\rfal_isoDep.h 278
Error[Pe079]: expected a type specifier D:\Project_Dir\Middlewares\ST\rfal\Inc\rfal_isoDep.h 695
Error[Pe090]: function returning function is not allowed D:\Project_Dir\Middlewares\ST\rfal\Inc\rfal_isoDep.h 695
Error[Pe079]: expected a type specifier D:\Project_Dir\Middlewares\ST\rfal\Inc\rfal_isoDep.h 728
Error[Pe090]: function returning function is not allowed D:\Project_Dir\Middlewares\ST\rfal\Inc\rfal_isoDep.h 728
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1184
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1311
Error[Pe079]: expected a type specifier D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1786
Error[Pe090]: function returning function is not allowed D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1786
Error[Pe141]: unnamed prototyped parameters not allowed when body is present D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1786
Error[Pe042]: operand types are incompatible ("DSI_TypeDef *" and "enum #139") D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1792
Error[Pe031]: expression must have integral type D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1801
Error[Pe079]: expected a type specifier D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1818
Error[Pe090]: function returning function is not allowed D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1818
Error[Pe141]: unnamed prototyped parameters not allowed when body is present D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1818
Error[Pe042]: operand types are incompatible ("DSI_TypeDef *" and "enum #139") D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1825
Error[Pe031]: expression must have integral type D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1834
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1916
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1936
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1972
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1977
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1983
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 1987
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 2036
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 2042
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 2074
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_isoDep.c 2087
Error[Pe018]: expected a ")" D:\Project_Dir\Middlewares\ST\rfal\Inc\rfal_nfcDep.h 315
Error[Pe079]: expected a type specifier D:\Project_Dir\Middlewares\ST\rfal\Inc\rfal_nfcDep.h 315
Error[Pe168]: a function type is not allowed here D:\Project_Dir\Middlewares\ST\rfal\Inc\rfal_nfcDep.h 315
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_nfcDep.c 1846
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_nfcDep.c 2161
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_nfcDep.c 2169
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_nfcDep.c 2169
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_nfcDep.c 2203
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_nfcDep.c 2222
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_nfcDep.c 2225
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_nfcDep.c 2238
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_nfcDep.c 2240
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_nfcDep.c 2328
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_nfcDep.c 2402
Error[Pe134]: expected a field name D:\Project_Dir\Middlewares\ST\rfal\Src\rfal_nfcDep.c 2406
Any help would greatly be appreciated.
Solved! Go to Solution.
2018-10-10 07:26 AM
Hi,
after finding that there is DSI block on STM32F469 which does not exist on STM32F401 I assume that really this is the reason. DSI being defined by your BSP.....
Regards, Ulysses
2018-10-10 06:50 AM
Hi Andrew,
hard to judge. My blind guess would be that the STM32F469II brings a define for MBL, rendering the previous line in way that it requires more data for its statement.
Maybe you search for an MBL in the MCU support code.
If this does not help I recommend to make use of the -E option of the compiler to create the preprocessed files of the rfal_isodep.c . There it should be easy to see what actually happens.
BR, Ulysses
2018-10-10 07:26 AM
Hi,
after finding that there is DSI block on STM32F469 which does not exist on STM32F401 I assume that really this is the reason. DSI being defined by your BSP.....
Regards, Ulysses
2020-03-06 01:10 PM
The problem is that DSI(Display Serial Interface) is defined in BSP and in rfal library as well.
Maybe change the rfal DSI to something else(DSIx)?
2020-03-09 01:30 AM
Hi,
rfal just uses DSI as a member of a struct. BSP is kind of yielding the sledge hammer:
#define DSI ((DSI_TypeDef *)DSI_BASE)
Probably best to try to use "#undef DSI" in platform.h.
Regards, Ulysses