2018-10-09 05:07 AM
Hello,
I am working on a project based on NFC energy harvesting application. I am using AMS AS3955 dynamic tag which offers this functionality with ST25R3911B as the reader. In the ST25R3911B datasheet, it says that NFC type 4 tags are preferred and nothing is mentioned about other tag types.
Can ST25R3911B work with T2T commands(read/write)? If no then please suggest an alternative.
PS: AS3955 can also work on ISO14443A standard, but its mode must be changed to tunneling.
Thank you in advance!
Solved! Go to Solution.
2018-10-09 08:03 AM
Hi,
from ST25R3911B chip perspective you can use AM or OOK(bit tr_am is an independent bit). However when using AM for ISO14443A you may/will fail standard compliance (wave shapes). Some/many tags may understand some strong AM modulation as well.
Regards, Ulysses
2018-10-09 06:55 AM
Hi,
the AS3955 always works in iso14443a standard. Depending on the selected mode it can emulate an NFC type 2 (Level 3 by HW) or NFC type 4 (Level 4 by MCU software) tag.
ST25R3911B supports of course all ISO14443A protocol. Not sure where you find a mention of type 4 in its datasheet. If you happen to look at the ST25R3911B-DISCO software you will find some direct support in the mifare_ul.* files.
Regards, Ulysses
2018-10-09 07:25 AM
@Ulysses HERNIOSUS_O
Thank you sir for the clarification.
I just want to confirm one more thing please, so by working on ISO 14443A standard I can only go for OOK Modulation, isn't it? Or can I use AM modulation as well for the communication?
Sorry for the inconvenience. Thanks in advance for all the help.😊
2018-10-09 08:03 AM
Hi,
from ST25R3911B chip perspective you can use AM or OOK(bit tr_am is an independent bit). However when using AM for ISO14443A you may/will fail standard compliance (wave shapes). Some/many tags may understand some strong AM modulation as well.
Regards, Ulysses
2018-10-09 08:10 AM
@Ulysses HERNIOSUS_O
I want to maintain a constant field for energy harvesting. I think I got your point.
Thank you for the help.😊