cancel
Showing results for 
Search instead for 
Did you mean: 

How to load an user defined external loader in ST-Link

pese
Associate

I have created an external loader for S29GL032 NOR FLASH using STM32F051 as target.

The code in "loader_SRC" is rewritten from M29W128GL_STM3210E-EVAL project for TrueStudio using GPIO direct insted of FSMC.

The problem is that I can't see the loader (after renamed it with the right extension) in ST-LINK even though I can see it in the right directory containig all .stldr files and all examples

1 REPLY 1

The tools are sensitive to the content and layout of the ELF file sections, and the structure describing the part.

The STM32 ​Cube Programmer is also sensitive to an exact name match on the file vs part description.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..