cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F769I_EVAL: Camera stop streaming whenever I create a JPEG file into SD card

mthanh2602
Associate II

Hello

I'm a newbie as STM32. I want to write a program can take picture from camera and save it into SD card when I press a button.

I had finish this, but it's still having problems. The program stop after created one picture, after only one click. I can do it again by call initialize camera one more time.

I had found the cause is because "f_open" command. I try to run program like this below.

..........

..........

--Start camera and display on LCD---

loop{

->wait for the button was pressed.

if(FATFS_LinkDriver(&SD_Driver, SDPath) == 0) //1

    {

     if(f_mount(&SDFatFs, (TCHAR const*)SDPath, 0) == FR_OK)

     {

      f_open(&JPEG_File, "image.jpg", FA_WRITE || FA_CREATE_ALWAYS);

      f_close(&JPEG_File);

  }

 }

}

The camera stop even I didn't do anything. Just creating JPEG file and closing it after pressed the button.

Trying to understand the f_open() function, I think it's related to the line "stat = disk.drv[pdrv]->disk_initialize(disk.lun[pdrv]);" into the function disk_initialize() of diskio.c.

When I ignore this line, camera didn't stop. But I still really don't understand what happened.

Anyone know about this problems, please tell me. Why the camera is stop when I create JPEG file, and what should I do for dealing with this problem.

Thanks so much.

0 REPLIES 0