cancel
Showing results for 
Search instead for 
Did you mean: 

I can not launch it after I installed on windows 10

Allen Lin
Associate II

Hi,

I just can see a flash of CubProgrammer when I double click its short-cut icon. I have re-installed it several times. It always can give me a flash.

My OS is windows 10 and JAVA version is JRE 8. The java environment setting is

Path: C:\Program Files\Java\jre1.8.0_181

JAVA_HME = C:\Program Files\Java\jre1.8.0_181

The returned information of java -version is

java version "1.8.0_181"

Java(TM) SE Runtime Environment (build 1.8.0_181-b13)

Java HotSpot(TM) 64-Bit Server VM (build 25.181-b13, mixed mode)

Thank you for your helping.

Best Regards,

Allen

2 REPLIES 2
Allen Lin
Associate II

Hi All,

I find the root cause. It installs at JKD 11 when I install CubeProgrammer first time. But It still installs at JDK 11 after I install JRE 8 and set the path and JAVA_HOME for JRE8. It works well after I remove JDK11

Bertrand1
Senior

I confirm I had JDK10.2 installed and was unable to launch STM32CubeProgrammer v1.2..

Thanks for your post.

Bertrand