2018-09-30 11:34 PM
Hi , I encountered an interesting problem while I was trying to calculate the Bit-Banding Address of GPIO registers .
The peripherals working on AHB2 and AHB3 busses are overflowing when trying to calculate their bit-banding map .. For Example ;
I wanted to ease the syntax of reading some IO pins and here is the result for GPIOA , IDR register..
--------------------------------------------------------------------------------------
PERIPH_BASE =0x40000000
Address offset of IDR is = 0x10
AHB2PERIPH_BASE=(PERIPH_BASE + 0x08000000)
GPIOA_BASE =(AHB2PERIPH_BASE + 0x00000000)
GPIOA_BASE=0x48000000
---------------------------------------------------------------------------------------
For GPIOA_IDR_Bit0;
GPIOA_IDR_Bit0=0x42000000 + ((GPIOA_BASE +0x10-0x40000000)*0x20);
GPIOA_IDR_Bit0=0x142000200 .... Which is out of 0x42000000 -- 0x43FFFFFF Range !
Is there something I misinterpret ? or This is the reality of bit-banding exception such that doesn't work on some peripherals ... ?? Please tell me the truth .. I can live with that 🙂
Solved! Go to Solution.
2018-10-01 03:03 AM
AHB2 and AHB3 is not within the bit-banded peripheral area, which is 0x40000000-0x400FFFFF. See Bit-banding chapter in PM0214.
JW
2018-10-01 03:03 AM
AHB2 and AHB3 is not within the bit-banded peripheral area, which is 0x40000000-0x400FFFFF. See Bit-banding chapter in PM0214.
JW
2018-10-01 03:33 AM
So I have to go with RMW instructions for bit operations ? No other chance ?
2018-10-01 04:37 AM
No, but for example GPIO has it's own atomic write register, BSRR.
JW
2018-10-01 10:16 AM
Can you give me an example ?
2018-10-01 10:52 AM
GPIOA->BSRR = 0x00000001; // Set bit 0 (PA0)
GPIOA->BSRR = 0x00010000; // Clear bit 0
or *((uint32_t *)&GPIOA->BSRR) on platforms where BSRR/BRR are split in the structure definition
*((uint32_t *)&GPIOA->BSRR) = 0x00000001; // Set bit 0 (PA0)
*((uint32_t *)&GPIOA->BSRR) = 0x00010000; // Clear bit 0
2018-10-01 12:52 PM
Thank you so much Clive !