2018-09-29 07:54 AM
Hi,
I suspect that I encountered with undocumented silicon error of STM32L432KC, while I'm playing with a Nucleo32-L432KC board. Here is how to reproduce it:
In short, GPIO operation of PA5 (whose alternate function includes SCK) affects SCK of SPI1 (PA1).
Thanks,
2018-09-29 09:33 AM
Does same behavior occur if you manipulate PA5 by writing the the control registers directly, rather than using the HAL?
2018-09-30 11:28 PM
It's extremely unlikely you will find a silicon error when you're using HAL. If you find an error, it's an error in the HAL.
Create a bare metal example to validate the silicon error, I don't think there is one.
2018-10-01 04:43 AM
@Rob.Riggs Yes I'm manipulating the register directly. Could that be the reason?
2018-10-01 04:47 AM
Read out and post the relevant GPIO (and maybe also SPI) registers' content for the non-working case.
2018-10-01 05:12 AM
Here is GPIO setting for SPI generated by the CUBE
void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi)
{
GPIO_InitTypeDef GPIO_InitStruct;
if(hspi->Instance==SPI1)
{
/* USER CODE BEGIN SPI1_MspInit 0 */
/* USER CODE END SPI1_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_SPI1_CLK_ENABLE();
/**SPI1 GPIO Configuration
PA1 ------> SPI1_SCK
PA6 ------> SPI1_MISO
PA7 ------> SPI1_MOSI
*/
GPIO_InitStruct.Pin = GPIO_PIN_1|GPIO_PIN_6|GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* USER CODE BEGIN SPI1_MspInit 1 */
/* USER CODE END SPI1_MspInit 1 */
}
}
Then I control the PA5 this way
#define LED_OFF (GPIOA->BRR = GPIO_PIN_5)
#define LED_ON (GPIOA->BSRR = GPIO_PIN_5)
Whether I use HAL for the GPIO control or not, it is different pin isn't it?
2018-10-01 05:38 AM
2018-10-01 06:18 AM
Read out and post the relevant GPIO (and maybe also SPI) registers' content for the non-working case.
JW
2018-10-01 06:31 AM
Just for the purpose of record, I solved this problem by not using PA5. Maybe I'll get back to this and submit a whole project when I have time.