cancel
Showing results for 
Search instead for 
Did you mean: 

Atollic error "cannot find -l:libmc-truestudio_M0.lib" with STEVAL-SPIN3201

JLax
Associate

I am using the Motor control Workbench 5.1.0.18254 to generate an Atollic project for SPIN3201 eval board. When I try to generate the project, it does not find the following library "cannot find -l:libmc-truestudio_M0.lib".

I think the problem is that this library is not in the repository that generates the project "C:\Users\***\STM32Cube\Repository\MCSDK_v5.1.2-A1\MotorControl\lib".

Do I need to update the Motor Control Workbench application?

Best Regards

Jorge

1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards