cancel
Showing results for 
Search instead for 
Did you mean: 

When will STLINK-V3 and MB1440 become available?

Philipp Krause
Senior II

TN1235, released this month has some basic information on the new STLINK-V3 (which already can be ordered at some distributors, but lead times are long, and where there are pictures they show the older ST-LINK/V1)

According to TN1235, for the SWIM interface (and thus for using STLINK-V3 with STM8) one needs some adapter board called MB1440. I found no mention of MB1440 outside of TN1235.

When will STLINK-V3 and MB 1440 become available?

Philipp

5 REPLIES 5
martonmiklos
Senior
S C
ST Employee

More information will come mid-october​

Philipp Krause
Senior II

I received a note from someone who bought it at Mouser. Apparently, the STLINK-V3SET comes with the MB1440 included.

Philipp

Philipp Krause
Senior II

Images and link to USB data on a blog (not mine):

http://users.atw.hu/balubati/blog/index.php?entry=entry181002-114748

Philipp

martonmiklos
Senior

@S C​ 

It is a nice piece of hardware, with excellent capabilities!

Do you know if the protocol for the direct access of the USB-CAN, USB-I2C, USB-SPI will be published?

Documentation to the standard programming capabilities JTAG, SWD, SWIM would be very useful as well. (If not we have to reverse engineer it ;))