2018-09-14 04:45 AM
I want use to use a stm32L011 nucleo borad without a PC. Once the code is downloaded I want just supply the power of the nucleo board through the USB port with a single USB charger.
When I did it, the nucleo board doesn't start the code.
If I supply the nucleo borad through the USB port with a PC USB, the code works.
Why ?
And how to solve it?
Thanks in advance for your answers
BR
Serge Lopze
2018-09-14 04:54 AM
2018-09-14 07:58 AM
Hi Clive,
I found the solution to this. The solution documented on the ST's document : UM1956 - User manusl STm32 Nucleo borad page 16 ,§ 6.4.1 the note at the bottom of the page. (DocID028406 Rev3-
"In case the board is powered by a USB charger, there is no USB enumeration, so the LED
LD2 remains set to off permanently and the target STM32 is not powered. In this specific
case the SB1 must be set to on, to allow the target STM32 to be powered anyway.
"
I apologize to you for the distrub. At the end I learnt : I should be less layz and read better the specs that iI did until now.
Thanks for your answer
Have a nice week end.
Serge
2018-09-14 08:41 AM