2018-09-13 08:08 AM
I am trying to convert a signal from accelerometer to a digital value. The output coming from accelerometer is in mv so I have added a non inverting voltage amplifier, then too I am getting a dc voltage at the output of opamp so I have added two capacitors to eliminate dc voltage in my signal. Here are my issues,
When I tried have connected a potentiometer and tried, I didnt find any issues, ADC is working perfectly but when I am trying to connect the output from the capacitor to PA1 and ground, I could not able to get the reading from controller!!!! I mean the voltage across capacitor is dropping to mV . I have measured the voltage across capacitor in oscilliscope by not connecting to PA1 its working perfectly, peak to peak is coming at 4V when vibrating.. but the moment I connect the ouput from capacitor to PA1 and measure the voltage across PA1 to GND. its dropping to mV in which i cannot do the data acquisition.
Are there any hardware connections/ biasing I need to do for acquiring an AC signal?
I am using a STM32F429 discovery board, Keil, ADC is in interrupt mode. Kit is powered through USB via computer.
https://drive.google.com/open?id=1S_W7tXZgMwFcIQ1TJsEK5ybjGHp9yLB4
Solved! Go to Solution.
2018-09-17 11:13 AM
2018-09-13 08:42 AM
2018-09-13 09:37 AM
@Community member agreed for 3 V, any specific reason for voltage across PA1 to Gnd changing to mV as soon as I connect PA 1 to capacitor ? before connecting to PA1 voltage is around 4V.
2018-09-13 12:17 PM
2018-09-13 04:03 PM
To AC couple a signal to the ADC input you should bias the input with 2 2kohm resistors. One resistor is connected to ground and the other to 3V supply (reference )
The ADC sampling period should be adjusted for this source impedance.
Also limit your signal peaks to 0 to 3V max.
2018-09-13 11:13 PM
Capacitive coupling of the opamp output means you have the coupling capacitor and the S&H capacitor in series.
Not sure if this is what you want. Or stated differently, I'm sure this is not what you want.
2018-09-17 10:43 AM
@Community member , @Community member I have updated with a google link which opens the image of the schematics, I have removed capacitor after seeing the feed back. Then too the input driving to analog input goes to mV ( less than 300mV) as soon as i connect the analog input pin to the output of opamp.
2018-09-17 10:44 AM
@Community member In response to you post, I assume after some time in few seconds the ouput has to change. but it didnt.
2018-09-17 11:13 AM
2018-09-17 11:33 AM
@Community member you made my day.. I have been working on this for a week !!! thanks a lot!!! its working now.