cancel
Showing results for 
Search instead for 
Did you mean: 

ST25RU3993-EVAL Board + Tags

David3
Associate

Unable to get ST25RU3993-EVAL Board as it does not appear to be available, have all the details of board if we construct this Evaluation board would we be able to load the firmware into it and use the PC software and it work ok?

Second question, there are no ST UHF Tags available could not find any on ST site all the ones at any distributors (all obsolete) we have found some made by NXP I assume these will work with the ST25RU3993?

2 REPLIES 2
Bart Herse
Senior II

Hello,

boards are available please contact your local ST contact.

If you build the board exactly as is then the code will load and the board should work.

ST currently offers no Rain (UHF) tags.

The reader IC works with tags from other vendors.

Cheers,

B.

Raphael K
Associate II

Good day,

based on the ST25RU3993 and an STM32, we have built our own board with 8 antenna outputs. Is it possible to get the source code of the PC software (STSW-ST25RU001) so that we can extend it to 8 antennas?