2018-08-28 02:14 AM
Hi all,
I have a question about the full bridge driver L6207Q.
About the VREF signal, in my design I am going to drive it with a DAC with maximum output voltage above 1V.
I would avoid to insert an attenuation stage between DAC output and L6507Q VREF input.
Is advisable and , if yes, how much is possible to overcome the recommended maximum VREF level of 0,5V suggested in page 9 of AN1762?
My goal value for VREF max is around 0,7 - 0,75V. What kind of drawbacks I would face in this case?
Thanks for your attention,
Sergio
2018-09-07 05:29 AM
Hi Sergio,
the higher is the reference voltage, the bigger will be the power dissipation in the shunt resistors of the application . The 0.5 V indicated in the AN usually gives a good trade-off between power dissipation and sensing precision. However, your target value is still in a good region 😊
Regards
Enrico