cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F413VGT6 flash programming by ISP

GWu
Associate

​Hi All,

I am using a customized STM32F413VGT6(LQFP100) board, and try to programming flash by Embedded bootloader mode. The UART port is port 2, and boot mode is from system memory.

While I use ST flash loader to connect to the MCU, the flash loader cannot recognize the MCU as STM32, the Target chip become STM8.

And I use ST link to check if the chip is read protected, it is not.

I use UART command to get the MCU ID is 0x463, same as the description on user manual.

Does any one meet this issue? Thank!

0690X000006Bv1nQAC.png

0 REPLIES 0