cancel
Showing results for 
Search instead for 
Did you mean: 

Virtual EEPROM Linker Script Adjustments

HL?�t
Associate II

Hi,

I have some problems with setting up the virtual EEPROM on an stm32f405vgt6. I did not adjust the linker script and run into a hard fault. What I found out is, that the memory region of the flash, which I wanted to use for the virtual EEPROM, is already used by the microcontroller itself, such that I have to adjust the linker script. The problem is now, that I need sector 2 and 3 of the flash for the two 16kByte pages i want to use and this two pages are in between the flash and not at the end of the flash. So I need to adjust the linker script, such that it reserves me memory of sector 2 and 3, but I dont know how to achieve that.

What I imagine to do is something like this:

MEMORY
{
RAM (xrw)      : ORIGIN = 0x20000000, LENGTH = 128K
CCMRAM (rw)      : ORIGIN = 0x10000000, LENGTH = 64K
FLASH (rx)      : ORIGIN = 0x8000000, LENGTH = 32k
EMULATED_EEPROM (rwx) : ORIGIN = 0x8008000 LENGTH=2*16k
FLASH (rx)      : ORIGIN = 0x8008000+2*16k, LENGTH = 1024k-(32k+2*16k)
}

Such that I can split up the flash around my memory I use for the virtual EEPROM. How can I achieve that?

Datasheet:

https://www.mouser.ch/datasheet/2/389/stm32f405rg-956214.pdf

2 REPLIES 2

Correct you need to create a hole that the linker doesn't use.

The three flash regions would need to be uniquely named, with the vector table directed into the first.

FLASHBOOT (rx) : ORIGIN = 0x8000000, LENGTH = 32K

EMULATED_EEPROM (rwx) : ORIGIN = 0x8008000, LENGTH=32K

FLASHMAIN (rx) : ORIGIN = 0x8010000, LENGTH = 960K

Downstream script would need to direct objects and sections as required, linker isn't going to span

You might also consider having a separate boot loader and app, where the app gets the 960KB region starting at 0x08010000

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
HL?�t
Associate II

Thank you, that worked.