cancel
Showing results for 
Search instead for 
Did you mean: 

Low-Side Driver L9825

HIsma
Associate

Hi

I'm using L9825 in one of my applications and have couple of questions just to make sure I get it right:

1- I have Vcc=3.3v and Reset line pulled high. Is that ok?

2- my understanding is that NON1 and NON2 can be used to directly drive OUT1 and OUT2 independently of SPI interface; So after setting NON1 and NON2 to digital low/high, do I need to use the NCS line at all? anything else that I should consider?

Thank you.

0 REPLIES 0